5G NR
This topic describes the tabs in the area at the bottom of the Carrier screen.
This graphical display of the entire radio frame is located below the carrier, channel setup, and bandwidth part (BWP) property grids. This topic uses downlink as an example, but the information provided also applies to uplink.
It displays the resource allocation for each channel in a two-dimensional resource grid. The X-axis represents the slots, based on current numerology. The Y-axis represents the RB value. Each channel is assigned a unique color in the display. When you disable a channel, it no longer appears on the display.
View image.
Whenever you edit a parameter, the software automatically checks each carrier for resource conflicts. If a conflict occurs, an error message appears in the notifications area and in the notifications queue, describing the conflict.
View image.
The overlap between SS/PBCH and DL-SCH is allowed, the signal generation part avoids conflict automatically.
DMRS for different channels are not drawn on the graph.
This tab displays a table, summarizing all the parameter values for the carrier, various channel types or BWP. Select what you want to view from the buttons in the far left column.
View image.